Industry Online Support
Technical Forum
4/28/2006 6:07 PM | |
Posts: 19 Rating: (0) |
Hello, Is it possible to access a siwarex module, placed in an ET200-M, with SFCs (58 and 59) or you have to use I/O access only ?? Thanks |
4/29/2006 3:38 AM | |
Posts: 5822 Rating: (412) |
Hello tmm, I am not sure, but have you tried it with the ET 200 M configured as a S7-Slave yet? Best regards J_Bell |
4/29/2006 7:09 AM | |
Posts: 19 Rating: (0) |
The ET200-M is configured as DP-slave in a S7-300 system (master : CPU 314 with CP345-2). Thanks |
Follow us on