3/25/2018 1:57 PM | |
Joined: 9/28/2017 Last visit: 11/29/2023 Posts: 64 Rating:
|
Dear Friends, I am having a problem with one s7-300 system. The system consists of 313C CPU, four digital cards, and four analog cards. Now three of the analog cards has SF LED glowing. Other analog card doesn't have the SF LED. But the CPU has not any fault /maint LED glowing. Now the digital cards are working properly but the analog cards are not working. I have seen before that if the cards have any fault then the CPU will also show fault. I have checked the wiring and supply voltage to the cards. I am attaching the hardware config & diag as well as photo of the CPU & cards. Please help me to find the solution to run the system without any error. AttachmentHW_DIAG.zip (288 Downloads) |
3/25/2018 2:00 PM | |
Joined: 9/28/2017 Last visit: 11/29/2023 Posts: 64 Rating:
|
AttachmentSYS_PIC.zip (308 Downloads) |
3/25/2018 2:18 PM | |
Joined: 9/28/2017 Last visit: 11/29/2023 Posts: 64 Rating:
|
|
3/25/2018 3:55 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello RAKIB, did you make any changes to the system or did it suddenly appear? |
Follow us on