2/12/2020 12:49 PM | |
Joined: 3/2/2007 Last visit: 7/4/2024 Posts: 932 Rating:
|
is the below ET200SP interface the correct one to use with the TM timer module ? can we add also many normal input and output modules (digital and analog) to this rack, and also have the TM module work properly as fast output ? 6ES7138-6CG00-0BA0 , SIMATIC ET 200SP, TM timer DIDQ 10x 24V time-controlled digital inputs and outputs 4 DI, 6DQ withtime stamp Count, PWM,oversampling 6ES7155-6AU01-0CN0 , SIMATIC ET 200SP, PROFINET 2-port interface module IM155-6PN/2 High Feature, 1 slot for SIMATIC BusAdapter, max. 64 Periphery modules and 16 ET 200AL modules, S2 redundancy, Multi Hot swapping, 0,25ms isochronous mode, inclusive server module |
... thank you ... |
|
2/12/2020 1:04 PM | |
Joined: 5/12/2006 Last visit: 7/11/2024 Posts: 22308 Rating:
|
yes is the correct one. tm work as specified independed of additional other mopdules regards |
Follow us on