6/13/2016 3:15 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
@ Ayman, For me is like USB stick @ Jeffrey Other is, you see on the right the slot for SD Card? Try to save project with this slot, you need an SD card like 6AV6671-8XB10-0AX1, this is 512MB or Which external storage media can you use with the current SIMATIC ... like Ayman said the new and old panel have the same part number? Send to us the part number of the new, the old is on the attachment. |
Last edited by: Ste39 at: 6/13/2016 3:20:13 PM |
|
6/14/2016 3:17 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello Jeffrey, Ok the panel are the same, To backup the panel have you followed the procedure below descripted? How do you backup/restore with a Windows-based panel? - ID ... Or how did you do? |
6/15/2016 10:12 AM | |
Posts: 10 Rating:
|
Dear Sir, The Siemens PLC is the same, why cannot replace? That mean I need to order a new same model panel then do the setting ? Thank you Best Regards |
Follow us on