2/23/2006 4:12 PM | |
Joined: 12/5/2005 Last visit: 8/9/2021 Posts: 289 Rating: (19) |
Hi Salma. My problems are compounded by the fact that I'm not trying to debug one script. The animated objects areeach controlled by a script independently. The scriptsare very similar(in hind-sight, it would have been better to call a function to do the number-crunching). I've been working through one of the screens, and by a number of methods managed to get the initial update of the screen down to 15-20 seconds, but there is still a 7-10 second delay during which nothing seems to happen. I can try to post a copy of the screen here, if it helps. AttachmentMix-Tank.zip (505 Downloads) |
Follow us on