(0)| 5/26/2022 4:48 PM | |
|
Posts: 1 Rating:
|
Dear All, I have a question regarding the wiring of a 2-wire current transducer. 1, I can see on the circuit diagram in the manual the UV0..UV7 contacts provide 35V for the transducer. Is this true? Is it possible to adjust them for 24V? 2, Is it possible to use these inputs (I0+...I7+) with external 24V supply? In this case I only need to wire the I0+..I7+ contacts from the transducer and keep the UV0..UV7 contacts free? Thank you for your support! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/27/2022 10:19:40New subject after splitting |
|
Follow us on