(0)| 3/19/2025 4:45 PM | |
|
Joined: 11/6/2023 Last visit: 12/12/2025 Posts: 10 Rating:
|
Hi, sorry if I'm asking this in the wrong place but you were discussing HMI alarms. I am trying to create an analogue HMI alarm for oil level. The trigger would be when the level drops below a warning limit that would be set by the operator on the HMI. Therefore this limit could be variable and so I want to use a tag in the limit field of the analogue alarm. I have seen in older versions of TIA portal that this was possible but I am now using V19 with a Unified Comfort Panel. Is this no longer supported? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 03/19/2025 22:22:21New subject after splitting |
|
| 3/20/2025 12:03 PM | |
|
Joined: 7/11/2024 Last visit: 12/30/2025 Posts: 200 Rating:
|
Hi owenjpayne, Which issue are you facing in Unified V19? Can you elaborate a bit more? According to the manual, it is possible to work with analog alarms in V19 Configuring analog alarms Maybe this video can help you: Create HMI alarms (discrete & analog) Good luck! ✨ |
|
If this post has been useful, don't forget to rate it!😊 |
|
Follow us on