(0)| 3/25/2025 9:35 AM | |
|
Joined: 9/9/2014 Last visit: 9/10/2025 Posts: 5 Rating:
|
Hello zixie, based on your request, you'd like to manage kinematic movements using the following sequence of operations:
It's important to note that TO Kinematics only allows the motion queue to continue if the kinematics are in the exact position where they were interrupted initially. This requires moving the kinematic axes back to the position where it got interrupted by the MC_GroupInterrupt command prior to continuing. In order to facilitate this sequence more efficiently, we recommend using the LKinAddon_KinematicsSimulationSequence function block from the SIMATIC Kinematics Add-On library. This function block is specifically designed to manage such sequences. Here’s how it works:
For more detailed information and to download the library, please refer to following entry in SiePortal: SIMATIC Kinematics Add-On |
This contribution was helpful to
|
|
Follow us on