(0)| 4/4/2025 3:29 PM | |
|
Joined: 7/20/2023 Last visit: 4/10/2025 Posts: 25 Rating:
|
Hello I have the same problem. I got a battery error, I lost parameters only in the spindle. So I tried to put the arc files back in without success. The NCU won't let me reset the NC and PLC. It always flashes 1-0-9. Or if I turn the machine back on, all the LEDs are on and only one dot appears on the display. If I disconnect the memory card, 0-6 appears. Could it be that the card lost the software? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 04/07/2025 07:00:01New subject after splitting |
|
Follow us on