(0)| 1/14/2026 1:41 PM | |
|
Joined: 1/21/2025 Last visit: 1/15/2026 Posts: 3 Rating:
|
Hello, I am trying to set up a commusnicaton between Bender iso415r When I run my Modbus_Comm_Load I get no error, only state 16#0000 And Done Then when I try to read with Modbus_Master from address 1000 and length 1, I get the error 16#80C8. So also according the mentioned post, There is an issue in the G2 or the CB 1241. |
Last edited by: AutoGen_1866723 at: 01/14/2026 13:43:05Just a little change of line breaks for better readability. Last edited by: AutoGen_1866723 at: 01/14/2026 13:45:56Removed images, they were scaled down and unreadable. |
|
| 1/14/2026 2:03 PM | |
|
Joined: 7/31/2020 Last visit: 1/15/2026 Posts: 483 Rating:
|
Hello, The linked page indicates that the firmware can be updated using the Automation Tool. Required user action:
Best regards |
This contribution was helpful to
|
|
| 1/15/2026 7:58 AM | |
|
Joined: 7/31/2020 Last visit: 1/15/2026 Posts: 483 Rating:
|
Hello, The screenshot is too small, so the message is not legible. If the latest version of the Automation Tool is installed, it should work. In this case, you may want to contact technical support, referring to the entry in the post. Best regards |
Follow us on