10/20/2011 4:18 PM | |
Joined: 8/9/2011 Last visit: 5/27/2025 Posts: 324 Rating:
|
Dear All.. I have been facing this new hectic problem of late I have created one DB And created about 60 variables in total of REAL & WORD.I haven't used ull of them as i have kept them raedy for future. If i make all of them WORD This error appears & If i retain the original the problem comes So Please help me getting rid of it... Programe gets downloaded with no error... Thanks AttachmentNew WinZip File.zip (673 Downloads) |
Last edited by: GAJENDRADS at: 10/20/2011 4:34 PMPlease tell me what do you mean by that error? "Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
10/20/2011 4:36 PM | |
Posts: 270 Rating:
|
Hello GAJENDRADS, firstly to your problem. The error usualy means that you are trying to access (in this case with reading) an unmapped area of a DB. Note that REAL has 32 bits and hence is twice as long as WORD, which might lead into problem when you originaly call the values from DB and you are perhaps addressing way too high in your DB. More is covered in FAQ (http://support.automation.siemens.com/WW/view/en/23151678) and many other posts in the forum when you search the words of the error ("Area length error"). Secondly, when you make a screenshot and paste it into mspain(t), you can save it as some other formats than .bmp, overall .jpg(.jpeg)is nice for this, because it's not too big and still good quality wise. Why I say it - it's somewhat same size but the need for opening the .zip file might make some users (regarding to internal security policies) unable to open it. Anyway, hope some of this helps. |
10/20/2011 5:20 PM | |
Posts: 270 Rating:
|
Yes, that's the problem. |
This contribution was helpful to
1 thankful Users |
Follow us on