12/27/2011 3:33 PM | |
Posts: 25 Rating:
|
I have similar problem, the diagonostic file is attached. 1 of 22; Event ID: 16# 02:4000 CPU info: New startup information Pending startup inhibit(s): - Internal load memory is corrupt (delete in TIA Portal or with program card) - Parameter assignment error pending - Consistency error (load missing block or hardware configuration) - Operating mode change not allowed while loading the HW configuration Current CPU operating mode: STOP I have seen this problem in forum long time before, but now anyone know the correct solution to avoid it? I wonder if I could continue use S7-1200, even now have SP2 and V2.2. In fact, SP2 is faster and more mature, but I still got crash everyday. AttachmentDiagnostics.zip (666 Downloads) |
Last edited by: O_Moderator at: 12/28/2011 12:29 PMnew subject after splitting from /tf/WW/en/Posts/67278#top |
|
12/28/2011 2:22 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating:
|
Do you also use interrupt with some retain var, as Bigx does? How many retain vars do you use? |
Follow us on