(0)| 2/7/2014 12:01 PM | |
|
Posts: 16 Rating:
|
Thank you I am using WinCC flexible 2008 SP3, I will connect 2 PLC's with an ethernet switch. |
| 2/8/2014 9:15 PM | |
|
Posts: 895 Rating:
|
... 6 axis aren`t a problem with a S7-1200. You can use SINAMICS G120 drive with a CU250S. So you can use the basic positioner inside the CU250S and send the setpoints over PROFINET. In the following link you will find the "FB284": http://support.automation.siemens.com/WW/view/de/68034568 If you want to use a SINAMICS S drive (with CU305 for example), they would be the same FB284. |
Follow us on