(0)| 10/10/2008 2:27 PM | |
|
Posts: 39 Rating:
|
Hello hefeng_05 With the cam tool you can provide or examine the cam profiles only in offline mode. These cams will transfer with the SIMOTION SCOUT into the controller. In the controller the cams are synchronized and processed by the command _enablecamming. The functions of the cam tool are described in the following document: http://support.automation.siemens.com/WW/view/en/23988540 The handling of the cams in the controller (e.g. synchronization to the master) is described in the following document: http://support.automation.siemens.com/WW/view/en/28017268
ThomasD |
Follow us on