1/8/2009 11:29 PM | |
Posts: 1 Rating:
|
I have been requested to investigate, anda schemehas been created but I'm unsure if it will work. All inputs are greatly appreciated. The MM440 is being supplied with an AOP and a Profibus Module. The 3-Positon selector switch, Hand-Off-Auto, will switch control between the AOP and Profibus. When in OFF it will disable control from the AOP and Profibus. I have provided a diagram to illustrate. P0700[0] = 1 P0700[1] = 6 P0701 = 4 P0705[0] = 99 P0705[1] = 99 P1000[0] = 1 P1000[1] = 6 P0810 = 722.4 Am I doing something wrong? Thanks in advance, emang AttachmentMM4_AOProfi.pdf (365 Downloads) |
Last edited by: emang at: 1/8/2009 11:32 PM |
|
Follow us on