5/25/2021 1:58 PM | |
Joined: 3/30/2020 Last visit: 8/14/2024 Posts: 4695 Rating: (974) |
Hello. In a way I echo what mopS04 said. The help system runs on 32-bit based program that is not available in 64-bit Windows. Also Win7 will be a problem. There are ways of making the help work under Win7, but I do not know if the resource is still available to the public. WinXP is the best to use. My doubt comes from the ability to make PC and PLC link to each other. My copy of MicroWin does not work on Win10 anymore. You will have to check. As to the question.. you are able to get all information from the System Manual. This is highly recommended even if the help system did work. The download PDF is here: ~ |
Last edited by: qwazee at: 05/25/2021 13:59:07Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to2 thankful Users |
Follow us on