Industry Online Support
Technical Forum
3/19/2009 5:14 AM | |
Joined: 9/27/2006 Last visit: 8/21/2024 Posts: 12279 Rating:
|
Hello Rizal; In Protool you can define "area pointers" that allow you to interface between your controller program and you operator panel. One such area pointer is called "job mailbox". PLC jobs include setting the date/time (synchronizing), acknowledging alarms from the PLC program...PLC job 51 controls which screen is displayed on the OP. Once PLC job 51 is setup in the OP, you can interface through your PLC program to control screen display. More information on area pointers can be found in the Online Help for protool and the protool manuals. Here is a FAQ that will guide you in this configuration. It also contains a sample program you can study and use for basis of your own OP and PLCprogramming. http://support.automation.siemens.com/WW/view/en/24229825 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/19/2009 5:16 AM |
|
3/19/2009 5:40 AM | |
Posts: 77 Rating:
|
can i simulate it? |
3/19/2009 7:57 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hello With Step5, I don't think. regards |
3/19/2009 8:36 AM | |
Posts: 77 Rating:
|
I mean, simulate it in Protool only. can i? |
Follow us on