3/23/2022 11:23 AM | |
Joined: 2/29/2016 Last visit: 6/7/2024 Posts: 40 Rating: (0) |
Hi, I am trying to control a tank level with 2 analog triggers How it should work is the pump runs until the upper level is reached, when the level drops to the lower level set point the pump will start and run until the upper level is reached. But I need to be able to adjust the set points from an HMI but I am unable to solve this issue Currently using ComfortSoft V8.2 and TIA Portal V17 update 2 I have attached a copy of my project so far Regards DM AttachmentLevel Trial 23-2-22.zip (496 Downloads) |
3/23/2022 1:10 PM | |
Joined: 12/18/2014 Last visit: 7/5/2024 Posts: 33302 Rating: (4124) |
In attachment the example.
AttachmentDesert Monkey.zip (567 Downloads) |
Follow us on