4/24/2022 8:28 AM | |
Posts: 3 Rating:
|
Hello friends, I want to select a motor with VFD. Can this motor be used with VFD, 1LE1501-2BB23-4AB4-Z_L19+L51+M11+Q02+Y52 (attached file)?? or i have to change some part of it ? Regards, Attachment1LE1501-2BB23-4AB4-Z_L19+L51+M11+Q02+Y52_datasheet_en.pdf (741 Downloads) |
4/24/2022 9:04 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, What is the application? How much speed variation range? i.e. minimum & max RPM? What is duty cycle? |
4/25/2022 12:15 PM | |
Joined: 10/11/2006 Last visit: 8/15/2024 Posts: 5892 Rating:
|
Hello, please use the desktop variant of Tia Selection Tool (https://support.industry.siemens.com/cs/ww/en/view/109767888) to dimension the converter and motor to your load cycle. Tia Selection Tool: Please insert an axis -> New Device -> Drive technology -> Drive dimensioning (>48V with SIZER integrated in the TIA Selection Tool) |
With best regards, |
|
Follow us on