5/14/2022 11:12 AM | |
Joined: 10/30/2019 Last visit: 9/3/2024 Posts: 7 Rating: (0) |
Hello Dears, Actually i have problem of the setpoint of the analog input that's greater than the setpoint that i give by 5 HZ for example if i give from the SCADA 25 HZ that's means 12 mA the current goes out from the PLC is ( 12 mA ) and reach to the drive ( 12 mA ) but the Frequency that i get on the drive's screen display is ( 30 HZ ) that's means 5 HZ greater than that i give the parameters that i set on the drive P719 = 2 , P756 = 2 , P757= 4 mA , P758= 0% , P759= 20 mA , P760= 100% P1000= 2 , P1070= 755 , P2000= 50 HZ Both of the dip switches are " ON " that's means i use ( mA as an analog setpoint ) Any recommendation else can i do ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/16/2022 09:25:53New subject after splitting |
|
Follow us on