6/3/2022 11:52 AM | |
Joined: 10/10/2005 Last visit: 7/24/2024 Posts: 1917 Rating: (136) |
Hello inder22, as I understand it is intended to store data one at a time that is retrievable and not to be overwritten during the process. There is an FAQ with an example program that can help you, at least in part. With the blocks from this library, you can save up to 12 different return values one after the other in a data block with the S7-1200/S7-1500.This program can of course be expanded further. In STEP 7 (TIA Portal) how do you buffer the return values of FBs and FCs one after the other in a DB? With best regards |
This contribution was helpful to2 thankful Users |
6/7/2022 12:31 PM | |
Joined: 4/12/2022 Last visit: 3/28/2024 Posts: 17 Rating: (0) |
Thanks! This give me option on how to store the process value |
Follow us on