9/20/2022 3:50 PM | |
Joined: 12/30/2021 Last visit: 7/24/2024 Posts: 8 Rating: (0) |
Hello, I have my logo on the cloud and I make a webpage to monitor my logo. I have several timers and Input and output. Every thing works online UNLESS the only weekly timer I have on my logo program. On my logo, my timer is set at 10:00 On my Amazon web service IOT I can see in the shadows that the number of this VM is 1000 so it's correct because I set the timer ON at 10h00 The problem is that on my webpage the fist digit (for the hours) is 16#10 and the second digits (for the minuts) is 16#0 So I don't know why I have a #16 before each digits... I put the logo and the LWE program attached. Also 3 screenshots. Someone know what I´m doing wrong? :( Attachmentlogo and LWE.zip (343 Downloads) |
9/20/2022 4:01 PM | |
Joined: 12/30/2021 Last visit: 7/24/2024 Posts: 8 Rating: (0) |
I use the LWE v1.1.1. and the logo softcomfort v8.3.1 |
9/21/2022 3:03 PM | |
Joined: 12/30/2021 Last visit: 7/24/2024 Posts: 8 Rating: (0) |
Perfect it's working !! Once again, thanks a lot Ixo65 |
This contribution was helpful to1 thankful Users |
Follow us on