10/5/2022 2:18 PM | |
Joined: 3/21/2022 Last visit: 9/13/2024 Posts: 4 Rating: (0) |
Hello Prof Frink and Murof, thank you very much for your reply's. It was very helpful! I have created multiple jobs in the scheduler, and I can even create a job for the ArchiveLogFile, without writing a script for it. So really easy! :) But now I have an additional question when I was creating the jobs: How do I change the field "Directory Name"? Right now the directory is default "Storage Card MMC" but we run the WinCC application on a PC instead of a Panel. I have chosen a MP377 19" for the right resolution as a device. I think the problem starts there but I don't know wat to select else. Perhaps someone can help me out? Thanks in advance again! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/06/2022 06:38:03New subject after splitting |
|
Follow us on