11/2/2022 9:19 PM | |
Joined: 9/21/2012 Last visit: 11/6/2024 Posts: 4193 Rating: (472) |
There is a ready made control block for Telegram 20. The link also has nice documentation for the Telegrams. SINAMICS S/G/V: Simple cyclic Funktions Blocks for Controlling a SINAMICS in TIA Portal But back to the problem, have you set the HW config of TIA, for the drive to have Telegram 20, and also in drive has to have Telegram 20 set top it. On the drive, it's easyest to use commissioning wizard to set all the needed parameters to run the motor. |
Last edited by: Jen_Moderator at: 11/03/2022 09:18:57Link optimized. |
|
11/3/2022 5:39 PM | |
Joined: 9/21/2012 Last visit: 11/6/2024 Posts: 4193 Rating: (472) |
Did you download the HW config according to this photo? |
11/3/2022 5:47 PM | |
Joined: 6/7/2022 Last visit: 8/30/2023 Posts: 7 Rating: (0) |
Yes |
11/3/2022 8:53 PM | |
Joined: 4/28/2015 Last visit: 10/8/2024 Posts: 81 Rating: (2) |
like this |
11/3/2022 9:06 PM | |
Joined: 6/7/2022 Last visit: 8/30/2023 Posts: 7 Rating: (0) |
thank, Seems to be correct |
Follow us on