12/25/2022 9:33 PM | |
Joined: 1/2/2017 Last visit: 7/23/2024 Posts: 285 Rating: (23) |
Hello, I have looked into your example and it is working as expected. I need small help from you. I'm new to logo 8, I used to work with PLC's for long time but not Logo. I have a project where I needs to be programmed exclusively in Ladder, the flowmeter gives pulses where each pulse = 0.15 m3, I have to calculate the flow rate m3/hour and accumulate the volume in m3 and display it in a web server page. The pulses I guess will depends on the pump and the water, I expect it to fluctuate a bit. 1- how make accurate calculation of the flow in this case 2- I could not manage to calculate the volume, in the FBD, I saw you used some markers to save the data, I could not find this option in ladder. 3- How can I define few tags to save my flow rate and volume to present them in the web server? could you help me with explanation or an example project? I appreciate any help I'm using Logo without display 6ED1052-2HB08-0BA1 Kind regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/26/2022 08:50:01New subject after splitting Disclaimer: While I strive to ensure that the content of posts and answers is accurate and complete, my posts and answers are provided “as is” and “as available.” Your use of my posts and answers content is entirely at your own risk. |
|
Follow us on