1/26/2023 3:14 AM | |
Joined: 1/26/2023 Last visit: 6/7/2023 Posts: 2 Rating: (0) |
Hi, We currently have a WinCC 7.0 SCADA with S7-300 and S7-200 PLC controllers. We would like to upgrade the server and the latest WinCC version. Does the latest WinCC version (V7.5 sp2) compatible with the existing PLC controllers? Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/26/2023 11:09:16New subject after splitting |
|
1/26/2023 6:27 AM | |
Joined: 10/11/2018 Last visit: 4/16/2024 Posts: 49 Rating: (2) |
Hello Jimmy, with S7-300 there shouldn't be a single problem. with S7-200 it's not that easy and you must use one method mentioned here: AttachmentWinCC_Communication_en-US_en-US.pdf (295 Downloads) |
Last edited by: Jen_Moderator at: 01/26/2023 11:15:01PDF attached from link. Link optimized. |
|
3/10/2023 12:34 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640)
|
Hello Jimmy.H I checked it in WinCC V7.5 Sp2 the comunication channel Profibus DP is still available in WinCC V7.5Sp2 the settings as described in WinCC can also still be done: LINK But I do not know if it still works in The Communication Manual it is also described: https://support.industry.siemens.com/cs/ww/en/view/109792585/139331496331 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on