2/6/2019 12:28 PM | |
Posts: 3 Rating: (0) |
Hi all, Where can I find the CPU 1500 's safety data (exactly CPU 1513F-1), such as MTTFD, DC, CCF and category or λdu ? Thanks in advance for the help! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/7/2019 8:44:01 AMNew subject after splitting |
|
2/7/2019 10:50 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi, MTBF values are also available in the lins in this entry: Mean Time Between Failures (MTBF) - list for SIMATIC products hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
2/12/2019 7:05 PM | |
Posts: 3 Rating: (0) |
Hi mops04, thanks for your help, but safety CPU are not referenced in this list for SIMATIC products regards, |
2/14/2019 4:26 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello FC_CIPEN; The SET team proposes Safety-related data for the Siemens F_CPUs using PFD and PFDh values. For users who would rather have them in MTTFd and DCav format, there are ways to establish a relationship between the 2 sets of data, through specific calculations. An easier way is to use a Safety Calculator, such as Sistema, to do the translation for you. For that purpose, Siemns' SET team proposes a VDMA format library to import CF-CPU data in programs such as Sistema. See the screenshot below. Safety Evaluation Tool offers VDMA 66413 neutral data interface https://support.industry.siemens.com/cs/ww/en/view/109750403 And look at this presentation: ISO 13849-1 PL Calculations Simplified - Robotic Industries AssociationWhen you open the CPU data for a Safety-related configuration, information is provided in terms of PDFh; but you can ask for the same data to be translated to MTTFd, DCav and CCF (depending on the configuration of the Safety function, through the "Determine MTTFd from blocks" selector). Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/14/2019 4:27:06 PMLast edited by: dchartier at: 2/14/2019 4:37:27 PM |
|
1/31/2023 12:28 AM | |
Joined: 4/7/2022 Last visit: 12/13/2023 Posts: 1 Rating: (0) |
http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=27832836&caller=view |
Follow us on