1/18/2023 1:31 AM | |
Joined: 7/24/2019 Last visit: 1/30/2024 Posts: 5 Rating: (0) |
Can you explain how you update Simatic NET? Is it from the DVD or from a SIOS download? What component did you update? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/18/2023 10:27:29New subject after splitting |
|
1/18/2023 12:22 PM | |
Joined: 8/12/2021 Last visit: 4/16/2024 Posts: 303 Rating: (28) |
Hi, Updates can be found on the support website.
|
If this Information really helps, you could use the Rate function |
|
2/2/2023 7:15 AM | |
Joined: 7/24/2019 Last visit: 1/30/2024 Posts: 5 Rating: (0) |
Customer is using WinCC V7.4 SP1 and SIMATIC Net V14. |
2/10/2023 11:57 AM | |
Joined: 8/3/2009 Last visit: 4/24/2024 Posts: 12854 Rating: (1639) |
Hello You can only use a comatible Version of SIMATIC NET to your used WinCC Version. If you want to use a very newer Version on the same system then you have to upgrade als WinCC: Check in Compatibility tool: https://support.industry.siemens.com/cs/ww/en/view/64847781 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on