2/2/2023 6:41 AM | |
Joined: 3/11/2019 Last visit: 5/8/2024 Posts: 1408 Rating: (255) |
Hi DNS_123, in general the firmware on the cpu 1500 is downwards compatible, so it is possible to use an older firmware in project. What you can try as a workaround: Download the project with TIA to the SIMATIC Memory Card directly. The new Cards for S7-1x00 can be used with standard cardreader. Plug in the SMC into the cpu afterwards and check if an online connection is possible. How do you create the project data for the SMC so that you can download the project to the S7-1200/S7-1500 CPU even without STEP 7 (TIA Portal)?-> Option 1: Download configuration directly to the memory card How do you load the project data if the version of the firmware installed in the S7-1500 CPU cannot be selected in the hardware catalog of your version of STEP 7 (TIA Portal)?regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
Follow us on