2/6/2023 5:29 AM | |
Joined: 3/11/2019 Last visit: 9/6/2024 Posts: 1569 Rating: (289) |
Hi, if you would like to delete the data from the SMC manually, you can use a standard card reader (only possible with the new SMC for S7-1x00!). Open in windows explorer and manually delte the file "S7_JOB.SYS" and the folder "SIMATIC.S7S". Do not "format" the SMC with windows. Do not delete hidden files and folders! You can also download the project to the SMC directly, so you do not need an online connection to the cpu. Plug the SMC afterwards into the CPU again. How do you create the project data for the SMC so that you can download the project to the S7-1200/S7-1500 CPU even without STEP 7 (TIA Portal)?regards sancruz |
Feedback appreciated, please rate |
|
Follow us on