3/8/2021 1:45 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello Rgirundi,
https://support.industry.siemens.com/cs/ww/en/view/109773213/70687471243
The debugger can also be started up later and linked to the system currently running.
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
3/8/2021 6:31 PM | |
Joined: 7/10/2017 Last visit: 10/29/2021 Posts: 4 Rating: (0) |
Hello Georg Berghof, thanks for the reply. the debugger already starts automatically and loads my variables from my VB code, the problem is that VB code itself did not load, instead, displays the following message "There is no source code available for the current location." And the count doesn't open. Regards, |
2/6/2023 6:09 PM | |
Joined: 4/19/2020 Last visit: 4/22/2024 Posts: 4 Rating: (0) |
Hello Rgirundi , If you already installed visual studio with higher version than 2008 then debug with that visual studio. |
Follow us on