2/22/2023 2:03 PM | |
Joined: 3/2/2007 Last visit: 10/16/2024 Posts: 938 Rating: (5) |
Kindly, can we replace the Sitop 6EP1437-3BA00 by the Sitop 6EP1437-2BA20 without issues? Because when we tried it, we noticed some strange behavior on the machine! 6EP1437-3BA00 , SITOP modular 40 A Stabilized power supply input: 400-500 V 3 AC output: 24 V DC/40 A *Ex approval no longer available* 6EP1437-2BA20 , SITOP PSU300S 40 A stabilized power supply input: 400-500 V 3 AC output: 24 V DC/40 A *Ex approval no longer available* |
... thank you ... |
|
2/22/2023 2:45 PM | |
Joined: 7/19/2022 Last visit: 10/18/2024 Posts: 403 Rating: (65) |
Hello Ziemens, Actually the ideal replacement for the 6EP1437-3BA00 is the 6EP3437-7SC00-3AX0. |
If this Information really helps, you could use the Rate function |
|
Follow us on