3/7/2023 6:45 AM | |||
Joined: 3/11/2019 Last visit: 4/24/2024 Posts: 1373 Rating: (242) |
Hi, there is also a description for this in the manual. SIMATIC S7 S7-1200 Programmable controller"If you are reusing a SIMATIC memory card that contains a user program, data logs, recipes, or a firmware update, you must delete the files before reusing the card. Use Windows File Explorer to display the contents of the memory card and delete the "S7_JOB.S7S" file and also delete any existing folders (such as "SIMATIC.S7S","FWUPDATE.S7S", "DataLogs", and "Recipes").
" regards sancruz |
||
Feedback appreciated, please rate |
|||
This contribution was helpful to3 thankful Users |
3/7/2023 3:22 PM | |
Joined: 11/13/2019 Last visit: 3/7/2023 Posts: 2 Rating: (0) |
Guys, Thank you very much for your advices !!! I owe you a beer !!! It's easier than I thought !!! |
Follow us on