3/7/2023 7:36 AM | |
Joined: 3/7/2023 Last visit: 8/15/2023 Posts: 1 Rating: (0) |
I have a problem in S7 300 CPU 314-2DP. The master I/O module few inputs are showing short with ground and Slave one module is showing all inputs and outputs are showing short to the ground. What are the possible reasons. Do I need to chnage the slave module? Thanks & Regards, Abdul Hannan Khan ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/07/2023 11:41:41New subject after splitting |
|
Follow us on