3/21/2023 7:44 AM | |
Joined: 6/18/2020 Last visit: 10/3/2024 Posts: 12 Rating: (0) |
Hi Ixo65, My PC details : IP : XX.175.113.14 Subnet : 255.255.255.0 Gateway :XX.175.113.1 My Logo PLC details : IP : XX.175.100.195 Sunet : 255.255.255.0 Gateway : XX.175.100.1 Note : XX is common on Both LOGO & PC. Due to my Process Plant constrains i cannot bring them on same subnet. LOGO PLC IP is pinging from the EWS PC , but when i try to go online its giving message as below: "The IP addresses of Your PC & the target LOGO are not in the same subnet.Logo Soft will try to add an additional local IP address , Do you want to continue?" Then if i assign additional IP address , No comms established. Can you please assist. Note : Configuring of PC & LOGO IP on same subnet not possible due to my plant constrains. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/21/2023 09:13:54New subject after splitting |
|
Follow us on