3/25/2023 4:06 PM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33883 Rating: (4215)
|
Hello Deumyster, at first welcome to the forum. Take a look at this Siemens FAQ: How do you set up an SMS in LOGO! ? |
3/27/2023 12:33 AM | |
Joined: 3/24/2023 Last visit: 7/1/2024 Posts: 14 Rating: (1) |
I reprogrammed the setup in diagram mode this time instead of network mode. I used the instructions from: How do you set up an sms in LOGO!? https://support.industry.siemens.com/cs/document/109816021 and used this document to show me how to do it: LOGO! 8 / LOGO! CIM / SINAMICS V20 https://support.industry.siemens.com/cs/ww/en/view/109806055 I think it is set up correctly except that the data mapping is all wrong. I haven’t dealt with bits, bites, and words since the 5” floppy disks went away. Since the original LOGO! I have been able to do all my projects without networking them. I can find exact examples of how to do the set up for blocks that are mapped to VM, but not for the simple task of using the I/Os. I know this should be trivial, but I’m just not getting it resolved. The CIM will transmit SMS because it sends out the power on/off SMS. One time I got it to transmit a SMS when I activated an input, but I don’t know how I did it and can’t duplicate it again.AttachmentCIM--LOGO!8 SETUP.xlsx (566 Downloads) |
3/27/2023 12:45 AM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33883 Rating: (4215)
|
See attachment. Maybe this help you to understand the VM memory. Take also a look in the Online Help, search for VM. AttachmentLOGO! Bit, Byte, Word and DWord.pdf (637 Downloads) |
Follow us on