3/14/2023 2:45 AM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263)
|
The 0BA0 has no firmware V1.83.x. The 0BA0 has firmware V1.82.x. If you only post here in the forum then became you no answer from Siemens. If you want an answer from Siemens then start a Support Request. I use https and it's not faster. For installing certificate take a look at the current manual, chapter 11.4. LOGO! manual |
3/14/2023 10:32 AM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263)
|
As I wrote in the other topic: No chance. And if the support says that there is no problem, then the information is wrong. The fact that loading an LWE project into LOGO! 8.3 takes much longer than loading the same project into LOGO! 8.2 has been criticized here in the forum from the start since LOGO! 8.3 was released. Depending on the type and scope, the projects run on a LOGO! 8.3 in different browsers with errors or not at all. I have found that. Take a look at this topic in the German speaking part of the forum: Ladezeit des LOGO Webservers bei RUN-Status extrem langeRead the post from the account "LOGO! Support". It's also a official statement of Siemens. |
This contribution was helpful to1 thankful Users |
3/23/2023 7:12 AM | |
Joined: 2/15/2021 Last visit: 11/14/2024 Posts: 18 Rating: (0) |
Any news ? Or any luck with certificate ? |
3/23/2023 7:29 AM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263)
|
My last post in this topic is just 9 days ago. And you hope of any news? |
4/12/2023 7:12 PM | |
Joined: 6/20/2020 Last visit: 10/22/2024 Posts: 44 Rating: (0) |
The problem is the same with the certificate, maybe even worse! I will try AutoGen_380038's proposal from this topic: https://support.industry.siemens.com/forum/fr/en/posts/logo-8-3-lwe-1-1-very-slow-at-card /288420
|
Last edited by: a.piquerel35 at: 04/12/2023 19:12:59 |
|
Follow us on