4/24/2023 9:42 AM | |
Joined: 5/6/2022 Last visit: 9/25/2024 Posts: 454 Rating: (90) |
Hi eirik0101, Yes, they are different cards. You need a specific card for each equipment, you can't use the same ones. Below, I share with you the links where you can find the necessary cards. In the case of Unified panels you can find these cards (SD Memory Cards): "SD memory cards, 512 MB, 2 GB to 32 GB for SIMATIC HMI Panels, HMI Unified and IPC" For your S7-1500 equipment you will need to use a specific S7 Memory Card like the one I show you in the following link: "SIMATIC S7 Memory Card, 12 MB" I hope this information is useful for you. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on