12/17/2023 9:57 AM | |
Joined: 7/5/2010 Last visit: 4/20/2024 Posts: 16 Rating: (1) |
I using EasyBuilder Pro V6.09.01.357 Build 2023.11.23. Thanks to distributor of weintek from multiprojekt.pl I have fixed drivers from weintek and in my opinion they works ok. For correct support of string in s7-1200 You have to set ascii variable as DBx_String1 and in drivers setting it shoud be set : Device Setting->Parameter Setting->Register Behavior->String Type-> No Fill. Then You can correctly display and input ascii string and there is no need for writing scripts in hmi. AttachmentDBn_String.zip (146 Downloads) |
Last edited by: viper_lasser at: 12/17/2023 09:58:16 |
|
This contribution was helpful to2 thankful Users |
4/24/2024 9:04 AM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7954 Rating: (162) |
New question published by Vinicius_wcv is split to a separate thread with the subject Read the string from the PLC and store it in a DataLog.. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on