5/19/2023 11:41 AM | |
Joined: 9/26/2022 Last visit: 4/26/2024 Posts: 1 Rating: (0) |
Hello, We are taking trends for room values(Pressure, Temperature and Relative Humidity). We have created offline trends for the data point, but we also use online trends to show the value Warning and Alarm High & Low Limits. The High and Low Limits are online trend logs but when the trend view definition is opened, sometimes they are showed and sometimes it does not show them. When the time bar is set to few weeks or months the High and Low Limits are loaded and they are shown and with zooming and manually navigating the time bar we can see the last day. But when we select 1 Day or 1 Hour on the time bar the High and Low Limits are not loaded and if the trend is not paused we can see the live values but they do not save. When we select the markers we noticed that the values are not logged periodically and they are missing. How can we set the logging interval for the online trend?
AttachmentTrendsInfo.pdf (446 Downloads) |
Follow us on