5/30/2023 10:55 PM | |
Joined: 5/30/2023 Last visit: 6/14/2023 Posts: 6 Rating: (0) |
Good estimates, I ask you about your project, I want to change the 1200 device for one that I have, only the HW version is higher than the one I have (4.0 to 4.4 available for the change and I have 3.1) How can I solve? Or is there no problem using a larger version?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/31/2023 08:09:46New subject after splitting |
|
5/31/2023 3:45 PM | |
Joined: 7/7/2010 Last visit: 9/19/2024 Posts: 15207 Rating: (2417)
|
My opinion: You do not have Firmware 3.1. You might have Firmware 3.0.1, which is read portal as FW 3.0 when selecting a PLC. If you add the FW 3.0 PLC with the exact same part # as you physically have to the project with the FW 4.x S7-1200 PLC, you can manually drag-and-drop (copy) tags, UDTs, blocks, and then manually configure the hardware to match what you really have. Once the FW 3.0 PLC project is configured, compile that PLC's hardware configuration - fix any problems. Then, compile the software and fix all the problems that come up. After that, download the FW 3.0 PLC project to the physical PLC.
|
science guy |
|
6/5/2023 2:13 PM | |
Joined: 5/30/2023 Last visit: 6/14/2023 Posts: 6 Rating: (0) |
Well, this is what I sent to the email. I have a recurring issue in the Siemens forum, but I haven't been able to find any solution, so I was told to submit my project to you. The problem is that when importing the WP321 library into TIA Portal 16, it displays an error message stating that I cannot compile it because it is password-protected. Thank you in advance for your assistance, and I look forward to your response. Best regards,
AttachmentET 200SP.zip (409 Downloads) |
Last edited by: Jen_Moderator at: 06/06/2023 07:41:35Link removed and file attached as .zip file. |
|
Follow us on