6/2/2023 5:48 AM | |
Joined: 1/21/2013 Last visit: 9/18/2024 Posts: 3114 Rating: (486)
|
Hi, You should take a look at the SMC operation manual. My experience with SMC stepper motor controllers is not that great, the only controller I have worked with was PROFINET enabled, so the controller offered more freedom to configure. However, in my personal opinion, these controllers are difficult to understand. As far as I could tell from my brief look at the manual, the controller allows you to configure 64 patterns of step data. This configuration must be written to the controller using the SMC PC software or a teach box. The PLC can select one of the steps by writing the step number to input terminals A3 - A8. Turning on A11 (DRIVE) will start the operation defined in the selected step. Of course, this will only happen if all preconditions are met. So the first thing you need to do is get familiar with this controller. Come back when you have S7 or TIA Portal specific questions. Kind regards |
Follow us on