(0)| 5/17/2022 10:39 AM | |
|
Joined: 4/12/2022 Last visit: 2/10/2025 Posts: 2 Rating:
|
Hi everyone, I also have a strange problem with the ID1000 values. I use it to count the pulses of an encoder, which seems to work fine in the sense that is shows me reasonable values on ID1000. For example, i rotate the shaft 360 deg and it shows 2500, which is the pulses per revolution of the encoder. So all seems fine until doing simple math with the value, which it does not respond to. I made the program as simple as possible to show the problem. (see attached image). When i simply add a random value (25 in this case) to the ID1000 value it seems to register the ID1000 as 0... It looks like a simple problem but i have been struggeling for over a day now. So please help. Thanks in advance! Kind regards, Mattias ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/17/2022 12:51:32New subject after splitting |
|
| 7/31/2023 9:23 AM | |
|
Posts: 2 Rating:
|
Thank you so much! Problem solved.
|
This contribution was helpful to
|
|
Follow us on