9/7/2022 2:52 PM | |
Joined: 5/20/2021 Last visit: 7/4/2024 Posts: 7 Rating:
|
The error is at the attachment. I try to connect with chrome to the IP address. I setup the IEM IP based, with DHCP, I create a NAT network to connect the IEM. And in the option during the installation that says Obtain hostname with DHCP I choose no. Here I read some post that is similar I think. similar error. |
Follow us on