8/19/2023 5:23 PM | |
Joined: 7/8/2023 Last visit: 8/22/2023 Posts: 8 Rating: (0) |
Hi again |
Last edited by: ALNR at: 08/19/2023 17:23:56Last edited by: Jen_Moderator at: 08/21/2023 08:19:16Text formatting optimized. |
|
8/19/2023 7:41 PM | |
Joined: 10/17/2007 Last visit: 7/14/2024 Posts: 4008 Rating: (353)
|
You save some steps, but waste our time and your time--why did NOT post NCU front Picture? However I need to know what kind of HMI you have. PCU50? or PCU20, or MMC103? check back of HMI to find it. and you need make sure your cable is in good condition. also I forget your story, you have had a good running machine, after battery low --you lost all parameter. or you got an 2nd hand machine you want to make it running? That will be dirrent story!
|
If you like my comments please |
|
This contribution was helpful to1 thankful Users |
8/19/2023 9:12 PM | |
Joined: 8/17/2023 Last visit: 4/30/2024 Posts: 30 Rating: (0) |
Hi,i have milling machine centre with 808d advanced siemens but i try to find battery,but seems there is no battery on my milling machine.i see in every zone but nothing....i have home reference aready set when i power the machine, so i dont' need to make zero point....is it possible that in my machine there isn't battery? |
8/19/2023 10:05 PM | |
Joined: 7/8/2023 Last visit: 8/22/2023 Posts: 8 Rating: (0) |
I apologize again I had a good running machine, after battery low --I lost all parameter and 120202 appear and the pr light go to off and ps , pf go to on. now after changing the battery and s3,s4 procedure, pr light is on but 120202 still appear my Hmi is pcu50. the cable seems good. |
8/20/2023 1:34 AM | |
Joined: 10/17/2007 Last visit: 7/14/2024 Posts: 4008 Rating: (353)
|
Ok, your NCU is ready for communication. then NCU<--->HMI conmmunication depending on following factors: #1--Cables --MPI cable if you don't touch I belive you they may be all good #2--Cable should connect to the right position/ connector--here, check your cable is connecting to X101--left top--(Siemens call OPI , transmmision baudrate is 1.5M) #3--the setting of NCK address inside NCK--if you cleaned NCK it should go back to default=13 #4--The setting in your PCU 50, --do like this go to Start-Up--> input password=SUNRISE dispaly will saying for MMC only (as you have no communication to NCK) answer OK, then the menu "MMC--> Opertaor Panel ---> here you can find setting --baudrate should be 1.5M, MMC address =1, NCK address=13. you can also press vertical menu "Load Standrad" after you have correct setting --save, then shut off machine power, then power up agian you will get communication if other factor all good please feedback here
|
If you like my comments please |
|
This contribution was helpful to1 thankful Users |
8/20/2023 1:59 PM | |
Joined: 7/8/2023 Last visit: 8/22/2023 Posts: 8 Rating: (0) |
I did everything you said But there is still message 120202 I took a series of photos of the work steps that I am sending I know I'm boring you, but please stay with me until I fix the problem Thank you ( I set the address to 12 once, the results are visible in the ((adress12)) pictures.) Attachment1.zip (299 Downloads) |
Last edited by: Jen_Moderator at: 08/21/2023 08:19:59Text formatting optimized. |
|
Follow us on