9/1/2023 6:11 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (821) |
Hello,
I see probably very basic problem, example use doesn't means that all will automatically working. there are many other specific cfg options that you need probably set and configure. Basic knowledge of ETH network, Modbus is required here, without doubts. PAC cfg check is required to see, what options are there and then you can set all also inside PLC to have all working. |
Last edited by: Duris_I at: 09/01/2023 06:13:37With best regards... |
|
This contribution was helpful to1 thankful Users |
9/2/2023 3:11 PM | |||
Joined: 3/29/2023 Last visit: 10/15/2024 Posts: 36 Rating: (0) |
|
||
9/4/2023 5:39 AM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (124)
|
Hi, In the manual and in the block online help it is described. Wüstenräuber |
This contribution was helpful to1 thankful Users |
Follow us on