9/13/2023 10:01 AM | |
Joined: 2/10/2015 Last visit: 5/16/2024 Posts: 286 Rating:
|
hi everyone, I use the compact PID block to read the volume of a tank, I called the PID in cyclic interrupt(OB30) and I use a PLC S7-1200(1214C AC/DC/RLY), but after configuring the compact PID, I see that nothing is working and all the outputs are at zero, and there I am stuck, I really need your help to understand why the block is not working in order to help me to solve the problem to get the desired operation. see attached file of what I did as configuration. thank you for helping me and best regards.
AttachmentPID.zip (308 Downloads) |
Follow us on