10/5/2023 10:33 AM | |
Joined: 10/5/2023 Last visit: 10/5/2023 Posts: 1 Rating:
|
Dear forum friends, I didn't want to open a new topic, as this is very similar or exactly the same of what i want. I have many serial working cncs using 840D sl or 840D pl, but on a new project i would like to test marking (date, time, etc.) to take place not in a different workcenter, but inside the CNC machine with a stylus tool (see attached, does not cut). What i want to engrave is also visible on the same attached pic. I read about cycle60, combined with R parameters (but this is mostly for increased No (n+1), also for PLC change SFC1 - SFC0, as well for GUD, ready cycles in softkey "engraving" (this is valid only for sl), lot of information. I would like help, By the way if you use stylus the spindle rotation is meaningless (?),does with cycle60 the spindle continue rotating or blocks in specific degrees (M19) and just scribe? Thank you in advance, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/13/2023 12:28:08New subject after splitting |
|
Follow us on