10/23/2023 3:08 PM | |
Joined: 3/9/2016 Last visit: 10/23/2023 Posts: 1 Rating: (0) |
Good afternoon, I am facing the same problem. Parameters set with the HMI ( and confirmed with OK) remain only valid as long the starter stays powered up. Once the power is cut, all changed parameters are lost. What is exactly the procedure to "lock the parameters" , as mentioned above? I can't find anything about this topic in the manuals. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/24/2023 09:02:42New subject after splitting. Quote inserted. |
|
10/24/2023 10:19 AM | |
Joined: 4/15/2009 Last visit: 7/8/2024 Posts: 123 Rating: (10)
|
Hi, Enclosed a manual extracts with the parameter. Best regards Sirius_3 AttachmentParameter of CPU.pdf (467 Downloads) |
Follow us on