10/20/2023 7:02 AM | |
Joined: 5/12/2006 Last visit: 9/2/2024 Posts: 22351 Rating:
|
and what eactly is the question now? |
10/27/2023 6:39 AM | |
Joined: 8/3/2009 Last visit: 8/15/2024 Posts: 13561 Rating:
|
Hello Vivek@Suryavanshi The question is which requirement is needed for access, if there should be a real client functionality with indipendent operating then this is not possible with WinCC Advanced RT. The WinCC Advanced RT is not real a SCADA solution like WinCC V7/8 or WinCC Prof. Its made for single monitor and single user situations. Also no Webbased application is available like in the other SCADA Products. Of course its a PC Based application, so you can have access with many ways like VNC, RDP, Teamviewer to the PC, But you will always only can remote control the PC/Runtime. Siemens offers also a VNC solution called SmartServer: https://support.industry.siemens.com/cs/de/en/view/109476153 Does this answer your question? if not, then please describe your usecase with more details. Bye Murof |
Last edited by: Murof at: 10/27/2023 06:39:46If this Information really helps, you could use the Rate function |
|
Follow us on